×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Honeywell MicroVCS: Game-Changing Cooling System Boosts Military Capabilities

Honeywell Attune: Game-Changing Cooling System Boosts Military Capabilities

High temperatures are a formidable enemy for today’s leading military aircraft, ground vehicles and naval vessels, which are packed with electronic systems generating a lot of heat. The problem is conventional cooling systems are often too big and heavy to cool sensitive electronics on defense platforms where size and weight really matter.

Enter Honeywell Attune. Building on our long legacy of thermal control technologies for military applications, Honeywell Attune (formerly known as Micro VCS) packs a lot of performance in a small, light and highly efficient package, according to Matt Milas, President of Honeywell’s Defense and Space business.

"Honeywell Attune addresses the size-weight challenge with a design that is significantly smaller and as much as 35% lighter than conventional systems,” Milas said. “This is truly a breakthrough technology that is poised to redefine the way defense platforms are cooled, which will enhance their mission readiness and ensure success in even the most challenging operating environments.”

Here are some other key benefits of Honeywell Attune and how it is revolutionizing the defense sector:

Light and Compact Design:

One of the most significant challenges in defense applications is the need to minimize weight and space requirements. Honeywell Attune offers a lightweight design that is particularly advantageous for aircraft, such as the F-35 Lightning II, F-22 Raptor, F-16 Fighting Falcon, and F/A-18 Super Hornet, along with ground vehicles like the M1 Abrams Main Battle Tank and Joint Light Tactical Vehicle (JLTV). Moreover, Honeywell Attune is engineered to fulfill the emerging requirements of the family of defense systems, which are presently being devised for 6th generation platforms.

Easy Integration:

Honeywell Attune is designed for easy integration into various defense platforms, making it a versatile solution for a wide range of applications. This adaptability allows it to be a potential enhancement solution for existing systems, reducing development time and costs.

Low Maintenance:

The system is highly reliable and virtually maintenance-free, thanks to its unique oil-free technology and small number of moving parts. This results in low total cost of ownership, allowing defense operators to focus on their missions without worrying about frequent maintenance.

Improved System Performance:

By maintaining optimal operating temperatures for electronics and avionics systems, Honeywell Attune ensures that these components perform at their peak efficiency, reducing the risk of system failures or malfunctions. This improved performance is critical in high-stakes defense missions, where every component must function flawlessly.

Enhanced Mission Endurance:

Honeywell Attune is 20% more efficient than conventional vapor cycle systems with comparable cooling capacity, thanks to its variable-speed compressors that maximize power efficiency by matching speed to capacity demand. This precise cooling helps reduce power consumption, which in turn can extend the battery life and overall mission endurance. This enhanced endurance is particularly crucial for unmanned aerial vehicles, where longer mission times can provide a strategic advantage.

Reduced Thermal Signature:

Efficient cooling enables the thermal signature of defense platforms to be minimized, making them less detectable by enemy sensors and improving their stealth capabilities. This is an essential advantage in modern defense operations, where evading detection can be the key to mission success. Honeywell Attune can contribute to stealth capabilities of aircraft and ground vehicles.

Increased Reliability:

The rugged design of Honeywell Attune ensures that it can withstand the harsh conditions often encountered during critical missions, such as high altitudes, temperature extremes, and vibration. As Milas states, "Honeywell Attune is built to endure the demanding environments of defense applications, providing our customers with a reliable and durable cooling solution across various platforms."

There is no doubt that Honeywell Attune is a transformative cooling technology that offers significant benefits to the defense industry, from weight and space savings to improve system performance and reliability.

Learn more about the Honeywell Attune cooling system here and explore how Honeywell’s strong legacy and relentless innovation are helping U.S. and allied forces achieve their missions.